Other Parts Discussed in Thread: ADS114S08, , ADS1220
Hi.
I need to design a common generic circuit for interfacing arbitrarily connected single-ended sensors which may have multiple ranges, such as 0-1V, or 0-2.5V or 0-5V. All signals will be single ended and unipolar.
The configuration of the registers can be controlled via SPI commands on a case to case basis. I do not want to make the ports rigid on the PCB end, like using opamps or jumpers, etc.
My AVDD=5V unipolar. This question is to check if i have understood the design correctly.
- First of all, the resolution will be limited to 15bits (1 bit lost due to unipolar PS and signals).
- PGA needs to be disabled for all these measurements.
- For, 0-5V signals i can just use AVDD-AVSS as the reference and a gain of 1.
- For V range between 0-2.5, i can use an external reference connected to REF0P and REF0N.. Can you recommend a 2.5 ref chip? or can i get away with a voltage divider?
- For a signal of 0-1V, I can use a gain of 2 and internal ref of 2.048, right?
- If I wish to measure a voltage swinging around 2.5V (1.5V lowest, to 3.5 highest), is there some shifting i can do to without using any opamps to optimize the measurement?
Finally, i was wondering if the ADS114S08 is a better IC as it has more ports and i can play with making the AINN part either connected to AVSS (for single ended unipolar measurements) or use the incoming signals refered to AINCOM which is further connected to the 2.5 Vref and thus achieve a single ended by bipolar measurement. Any recommendations will help me.
thanks!