This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADC14155QML-SP: Power Sequencing for VD and VA

Part Number: ADC14155QML-SP
Other Parts Discussed in Thread: ADC14155

Hello,

I am looking to understand if there are any power sequencing requirements on the ADC14155.  Particularly, will there be a problem if the part sees a VD of 3.3V and a VA of 0V for some period of time (on the order of tens of seconds). I see on the datasheet absolute maximum ratings that the difference between the two should be less than 100 mV.  Is there any risk of damage to the part if the two power supplies are not brought up at the same time, where VD = 3.3V and VA = 0 V for around 20 seconds?

Thanks,

Brandon