I want to obtain a demodulated signal of a continuous wave with a center frequency of 22 MHz. I want to obtain the Doppler frequency component on the baseband side through the LNA -> 3rd LP filter (30 MHz) ->ADC -> Digital Demod process. However, even if it is set as below, the LVDS output does not come out at all except 0.
Please check if there is a block that I forgot to disable to use the sequence like above.
cf) For the current progress, it was confirmed that the RAMP test pattern appeared through the LVDS output through the following setting.
SPI_DIG_EN = 1
1. Normal operation - At 0x00 address, transfer 16 bit data: 0x00 0x00
2. Disable demodulator: At 0x16 address, transfer 16 bit data: 0x00 0x01
3. Ramp signal: At 0x02 address, transfer 16 bit data: 0xE0 0x00