This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS1292ECG-FE: USB driver installation issue

Part Number: ADS1292ECG-FE

Hi there, 

I'm trying to connect the kit to my pcb, here are a list of steps that ive tried, but havent worked:

- when plugging the device into the PC, it is not recognised, drivers do not automatically install

- it doesnt show up in device manager

- navigating to the texas instruments folder, and trying to manually install the drivers from there by doubling clicking the executable file, also doesnt work 

- ive tried these steps on both windows 10 and windows 7 systems

- the only connection from the board is from the usb chord, no external power supply

- is there a link to the specific usb driver that i need, so that i can download it manually? 

Thanks!