This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS8685: Could ADS8685 support 8pcs in daisy-chain mode?

Part Number: ADS8685


Hi team,

Customer want to use ADS8685 in their project. They want to use 8 pcs in daisy chain mode, could you help if ADS8685 could support 8 pcs in daisy-chain mode? Thanks.

Best Regards,

Will

  • Hi Will,

    The data sheet does not specify the device quantity for the daisy-chain and it only shows an example with three devices in a daisy-chain in Figure 7-27. Based on support experience,  three or four devices in daisy-chain configuration should be fine. More devices in daisy-chain mode may lead to timing errors which will violate the setup parameter requirements and result in incorrect data capture by the host controller. Also, note that the overall throughput of the system is proportionally reduced with the number of devices connected in a daisy-chain configuration.

    Best regards,

    Dale