Part Number: ADS8168EVM-PDK
Other Parts Discussed in Thread: ADS8168
Hi
I would like samples to be negative when below Vref/2. Is this at all supported?
Somthing about this transfer function (without exact values)
-2.048 V = 0x8000
-0.001 V = 0xFFFF
0.000 V = 0x0000
0.001 V = 0x0001
2.048 V = 0x7FFF
If possible, then share jumper setting, sw setting and input signal pins / signal levels....
Regards
/Peter