Part Number: ADS124S08
I am using the ADS124S08 for a strain gauge design, things are going good, I can accurately read a typical 350 ohm strain wheatstone bridge sensor that is powered off of 5VDC with great performance with a VREF of 1.25V and a gain of 64.
Problem I am having is one of my sensor is a MEMS type bridge sensor that wants a constant current source. I am going the source but it results in a voltage between the Differential + and GND of 5V and a voltage between the Differential - and GND of 5V. I am not getting much count response from the ADC. The sensor is varying nearly 6 mV over the range and with a reference of 5V and a gain of 64 I should be getting allot of 23b counts. I am not I am only getting 100 or so. Am I missing something here on how this constant current sensor works?
Just making sure I am not violating an input rule of the ADC.
CMJ1500 TR PBFREE Central Semiconductor Corp | Integrated Circuits (ICs) | DigiKey is the link to the constant current diode I am using to provide the 1.5mA constant current supply.
ME501-5_DS_D-Metallux-SA-17062019.pdf is a link to the sensor I am using. it is a MEM501-A-0500-0-1-31-1