Part Number: ADC12DJ5200RF
Referring to Section 7.3.3.4 of the current datasheet, SLVSEN9B (page 71):
1. Please confirm that the ORA0, ORA1 pins are driven high even if one sample is above the OVR_T0, OVR_T1 threshold levels
2. Please confirm that if ORA0, ORA1 are driven high, that they stay high for the number of DEVCLK cycles set by OVR_N in Table 7-3
---- for instance, the ORA0, 1 pin essentially pulse stretches the configured number of DEVCLK cycles triggered from the last ORA0,1 event
3. If the ADC12DJ5200RF is operated in single channel mode at 5.2Gsps, is DEVCLK for the purposes of the above mentioned stretching time = 10.4GHz (per table 7-5)?
---- If this were the case, and let's say OVR_N = 7, then a single overrange sample on CHA would yield an ORA0,1 pulse length of 1024 * (1/10.4G) = 98.46nsec
---- or is it the case that a single overrange sample on CHA would yield an ORA0,1 pulse length of 1024 * (1/5.2G) = 196.9nsec
4. Let's say we are in JMODE 24 (CS=1, decimate by 8, single channel) sampling DES at 5.2GHz input clock. If we get an overrange, do the ORA0,1 bits still set AND the LSB of the of the Channel A samples is also set?
5. For the situation in "3&4" above, what is meant by the MONITORING PERIOD" as called out in Table 7-4?
--- Does this mean that when an overrange is detected, the decimated transport data LSB will "stretch" for 2^7 = 128 ADC samples? (Is that FCLK = 5.2GHZ or DEVCLK at 10.4GHz)?
Thanks!
Steve