Other Parts Discussed in Thread: LMK04828, LMX2592, LMH5401, ADC12DJ5200RF
ello,
We have an issue with the Foreground Calibration in the ADC12DJ2700.
Normally, meaning for JMODE_0, JMODE_2, foreground calibration passes.
Also, for JMODE_16 with sample clocks of ~2450 and higher, foreground calibration passes.
For JMODE_16, for lower sample clocks, mainly at ~2400MHz and lower, it fails.
Usually, FG_DONE bit polling took up to 400msec until successful FG calibration was detected.
We tried extending the time to few seconds what with no use. The failure is still there.
What can affect FG calibration failure in our case?
How should we debug this?
Background information:
In our design, the LMK04828 is used as the clock distribution device for the JESD204B DEVCLK and SYSREF,
which feeds a Xilinx FPGA (JESD204B receiver) and a LMX2592, which supplies the ADC12DJ2700 sample clock.
The system analog input goes to a LMH5401 diff opamp (SE input to DIFF outputs), which feeds the ADC12DJ2700.
Attached find the ADC register dump for JMODE_16, 2700MHz (FG calibration pass) and JMODE_16, 2200MHz (FG calibration fail).
=== ADC 2700 MHZ, Two Channel, X16 ====================================================================== ADC-12-DJ-2700 Registers ====================================================================== 0x000 - CONFIG_A: 0x30 0x002 - DEVICE_CONFIG: 0x00 0x003 - CHIP_TYPE: 0x03 0x004 - CHIP_ID_A: 0x20 0x005 - CHIP_ID_B: 0x00 0x006 - CHIP_VERSION: 0x0a 0x00C - VENDOR_ID_A: 0x51 0x00D - VENDOR_ID_B: 0x04 0x010 - USR0: 0x00 0x029 - CLK_CTRL_0: 0x60 0x02A - CLK_CTRL_1: 0x20 0x02C - SYSREF_POS[7:0]: 0x8d 0x02D - SYSREF_POS[15:8]: 0x31 0x02E - SYSREF_POS[23:16]: 0xc6 0x030 - FS_RANGE_A[7:0]: 0xff 0x031 - FS_RANGE_A[15:8]: 0xff 0x032 - FS_RANGE_B[7:0]: 0xff 0x033 - FS_RANGE_B[15:8]: 0xff 0x038 - BG_BYPASS: 0x00 0x03B - TMSTP_CTRL: 0x00 0x048 - SER_PE: 0x07 0x060 - INPUT_MUX: 0x01 0x061 - CAL_EN: 0x01 0x062 - CAL_CFG0: 0x05 0x06A - CAL_STATUS: 0x0b 0x06B - CAL_PIN_CFG: 0x00 0x06C - CAL_SOFT_TRIG: 0x01 0x06E - CAL_LP: 0x88 0x070 - CAL_DATA_EN: 0x00 0x071 - CAL_DATA: 0x00 0x07A - GAIN_TRIM_A: 0xb3 0x07B - GAIN_TRIM_B: 0xab 0x07C - BG_TRIM: 0x0b 0x07E - RTRIM_A: 0xa7 0x07F - RTRIM_B: 0xaf 0x080 - TADJ_A_FG90: 0xbf 0x081 - TADJ_B_F_G0: 0x80 0x082 - TADJ_A_BG90: 0xb4 0x083 - TADJ_C_BG0: 0x98 0x084 - TADJ_C_BG90: 0xe0 0x085 - TADJ_B_BG0: 0x80 0x086 - TADJ_A: 0x61 0x087 - TADJ_CA: 0x92 0x088 - TADJ_CB: 0x97 0x089 - TADJ_B: 0x80 0x08A - OADJ_A_INA[7:0]: 0xfc 0x08B - OADJ_A_INA[15:8]: 0x07 0x08C - OADJ_A_INB[7:0]: 0x85 0x08D - OADJ_A_INA[15:8]: 0x07 0x08E - OADJ_C_INA[7:0]: 0x8a 0x08F - OADJ_C_INA[15:8]: 0x07 0x090 - OADJ_C_INB[7:0] 0x6e 0x091 - OADJ_C_INA[15:8]: 0x07 0x092 - OADJ_B_INA[7:0]: 0x59 0x093 - OADJ_B_INA[15:8]: 0x07 0x094 - OADJ_B_INB[7:0]: 0x85 0x095 - OADJ_B_INB[15:8]: 0x07 0x097 - OSFILT0: 0x00 0x098 - OSFILT1: 0x33 0x102 - B0_TIME_0: 0x7a 0x103 - B0_TIME_90: 0x86 0x112 - B1_TIME_0: 0x80 0x113 - B1_TIME_90: 0x80 0x122 - B2_TIME_0: 0x76 0x123 - B2_TIME_90: 0x81 0x132 - B3_TIME_0: 0x80 0x133 - B3_TIME_90: 0x80 0x142 - B4_TIME_0: 0x83 0x143 - B4_TIME_90: 0x80 0x152 - B5_TIME_0: 0x80 0x153 - B5_TIME_90: 0x80 0x160 - ENC_LSB: 0x00 0x200 - JESD_EN: 0x01 0x201 - JMODE: 0x10 0x202 - KM1: 0x05 0x203 - JSYNC_N: 0x01 0x204 - JCTRL: 0x01 0x205 - JTEST: 0x00 0x206 - DID: 0x00 0x207 - FCHAR: 0x00 0x208 - JESD_STATUS: 0x7c 0x209 - PD_CH: 0x00 0x20A - JEXTRA_A: 0x00 0x20B - JEXTRA_B: 0x00 0x210 - DDC_CFG: 0x00 0x211 - OVR_T0: 0xf2 0x212 - OVR_T1: 0xab 0x213 - OVR_CFG: 0x07 0x214 - CMODE: 0x00 0x215 - CSEL: 0x00 0x216 - DIG_BIND: 0x00 0x217 - NCO_RDIV[7:0]: 0x00 0x218 - NCO_RDIV[15:8]: 0x00 0x219 - NCO_SYNC: 0x01 0x220 - FREQA0[7:0]: 0xb4 0x221 - FREQA0[15:8]: 0x97 0x222 - FREQA0[23:16]: 0xd0 0x223 - FREQA0[31;24]: 0x5e 0x224 - PHASEA0[7:0]: 0x00 0x225 - PHASEA0[15:8]: 0x00 0x228 - FREQA1[7:0]: 0x00 0x229 - FREQA1[15:8]: 0x00 0x22A - FREQA1[23:16]: 0x00 0x22B - FREQA1[31;24]: 0xc0 0x22C - PHASEA1[7:0]: 0x00 0x22D - PHASEA1[15:8]: 0x00 0x230 - FREQA2[7:0]: 0x00 0x231 - FREQA2[15:8]: 0x00 0x232 - FREQA2[23:16]: 0x00 0x233 - FREQA2[31;24]: 0xc0 0x234 - PHASEA2[7:0]: 0x00 0x235 - PHASEA2[15:8]: 0x00 0x238 - FREQA3[7:0]: 0x00 0x239 - FREQA3[15:8]: 0x00 0x23A - FREQA3[23:16]: 0x00 0x23B - FREQA3[31;24]: 0xc0 0x23C - PHASEA3[7:0]: 0x00 0x23D - PHASEA3[15:8]: 0x00 0x240 - FREQB0[7:0]: 0xb4 0x241 - FREQB0[15:8]: 0x97 0x242 - FREQB0[23:16]: 0xd0 0x243 - FREQB0[31;24]: 0x5e 0x244 - PHASEB0[7:0]: 0x00 0x245 - PHASEB0[15:8]: 0x00 0x248 - FREQB1[7:0]: 0x00 0x249 - FREQB1[15:8]: 0x00 0x24A - FREQB1[23:16]: 0x00 0x24B - FREQB1[31;24]: 0xc0 0x24C - PHASEB1[7:0]: 0x00 0x24D - PHASEB1[15:8]: 0x00 0x250 - FREQB2[7:0]: 0x00 0x251 - FREQB2[15:8]: 0x00 0x252 - FREQB2[23:16]: 0x00 0x253 - FREQB2[31;24]: 0xc0 0x254 - PHASEB2[7:0]: 0x00 0x255 - PHASEB2[15:8]: 0x00 0x258 - FREQB3[7:0]: 0x00 0x259 - FREQB3[15:8]: 0x00 0x25A - FREQB3[23:16]: 0x00 0x25B - FREQB3[31;24]: 0xc0 0x25C - PHASEB3[7:0]: 0x00 0x25D - PHASEB3[15:8]: 0x00 0x297 - SPIN_ID: 0x01 0x2B0 - SRC_EN: 0x01 0x2B1 - SRC_CFG: 0x0b 0x2B2 - SRC_TAD[7:0]: 0x0d 0x2B3 - SRC_TAD[15:8]: 0x93 0x2B4 - SRC_TAD[23:16]: 0x02 0x2B5 - TAD[7:0]: 0x00 0x2B6 - TAD[15:8]: 0x00 0x2B7 - TAD[23:16]: 0x00 0x2B8 - TAD_RAMP: 0x00 0x2C0 - ALARM: 0x01 0x2C1 - ALM_STATUS: 0x0a 0x2C2 - ALM_MASK: 0x00 ====== ADC 2200MHz , TWO Channel , X16 ====================================================================== ADC-12-DJ-2700 Registers ====================================================================== 0x000 - CONFIG_A: 0x30 0x002 - DEVICE_CONFIG: 0x00 0x003 - CHIP_TYPE: 0x03 0x004 - CHIP_ID_A: 0x20 0x005 - CHIP_ID_B: 0x00 0x006 - CHIP_VERSION: 0x0a 0x00C - VENDOR_ID_A: 0x51 0x00D - VENDOR_ID_B: 0x04 0x010 - USR0: 0x00 0x029 - CLK_CTRL_0: 0x60 0x02A - CLK_CTRL_1: 0x20 0x02C - SYSREF_POS[7:0]: 0x31 0x02D - SYSREF_POS[15:8]: 0x0c 0x02E - SYSREF_POS[23:16]: 0x83 0x030 - FS_RANGE_A[7:0]: 0xff 0x031 - FS_RANGE_A[15:8]: 0xff 0x032 - FS_RANGE_B[7:0]: 0xff 0x033 - FS_RANGE_B[15:8]: 0xff 0x038 - BG_BYPASS: 0x00 0x03B - TMSTP_CTRL: 0x00 0x048 - SER_PE: 0x07 0x060 - INPUT_MUX: 0x01 0x061 - CAL_EN: 0x01 0x062 - CAL_CFG0: 0x05 0x06A - CAL_STATUS: 0x0c 0x06B - CAL_PIN_CFG: 0x00 0x06C - CAL_SOFT_TRIG: 0x01 0x06E - CAL_LP: 0x88 0x070 - CAL_DATA_EN: 0x00 0x071 - CAL_DATA: 0x00 0x07A - GAIN_TRIM_A: 0xc9 0x07B - GAIN_TRIM_B: 0x4b 0x07C - BG_TRIM: 0x0c 0x07E - RTRIM_A: 0xac 0x07F - RTRIM_B: 0x6b 0x080 - TADJ_A_FG90: 0x57 0x081 - TADJ_B_F_G0: 0xc0 0x082 - TADJ_A_BG90: 0xbf 0x083 - TADJ_C_BG0: 0x2b 0x084 - TADJ_C_BG90: 0x3c 0x085 - TADJ_B_BG0: 0xc5 0x086 - TADJ_A: 0x40 0x087 - TADJ_CA: 0x00 0x088 - TADJ_CB: 0x80 0x089 - TADJ_B: 0xd3 0x08A - OADJ_A_INA[7:0]: 0x3d 0x08B - OADJ_A_INA[15:8]: 0x03 0x08C - OADJ_A_INB[7:0]: 0x04 0x08D - OADJ_A_INA[15:8]: 0x04 0x08E - OADJ_C_INA[7:0]: 0x40 0x08F - OADJ_C_INA[15:8]: 0x0b 0x090 - OADJ_C_INB[7:0] 0x0b 0x091 - OADJ_C_INA[15:8]: 0x04 0x092 - OADJ_B_INA[7:0]: 0x40 0x093 - OADJ_B_INA[15:8]: 0x00 0x094 - OADJ_B_INB[7:0]: 0x1c 0x095 - OADJ_B_INB[15:8]: 0x04 0x097 - OSFILT0: 0x00 0x098 - OSFILT1: 0x33 0x102 - B0_TIME_0: 0x40 0x103 - B0_TIME_90: 0x40 0x112 - B1_TIME_0: 0x40 0x113 - B1_TIME_90: 0x7f 0x122 - B2_TIME_0: 0xce 0x123 - B2_TIME_90: 0x07 0x132 - B3_TIME_0: 0x10 0x133 - B3_TIME_90: 0x40 0x142 - B4_TIME_0: 0x40 0x143 - B4_TIME_90: 0x14 0x152 - B5_TIME_0: 0x08 0x153 - B5_TIME_90: 0x04 0x160 - ENC_LSB: 0x00 0x200 - JESD_EN: 0x01 0x201 - JMODE: 0x10 0x202 - KM1: 0x05 0x203 - JSYNC_N: 0x01 0x204 - JCTRL: 0x01 0x205 - JTEST: 0x00 0x206 - DID: 0x00 0x207 - FCHAR: 0x00 0x208 - JESD_STATUS: 0x00 0x209 - PD_CH: 0x00 0x20A - JEXTRA_A: 0x00 0x20B - JEXTRA_B: 0x00 0x210 - DDC_CFG: 0x00 0x211 - OVR_T0: 0xf2 0x212 - OVR_T1: 0xab 0x213 - OVR_CFG: 0x07 0x214 - CMODE: 0x00 0x215 - CSEL: 0x00 0x216 - DIG_BIND: 0x00 0x217 - NCO_RDIV[7:0]: 0x00 0x218 - NCO_RDIV[15:8]: 0x00 0x219 - NCO_SYNC: 0x00 0x220 - FREQA0[7:0]: 0x45 0x221 - FREQA0[15:8]: 0x17 0x222 - FREQA0[23:16]: 0x5d 0x223 - FREQA0[31;24]: 0x74 0x224 - PHASEA0[7:0]: 0x00 0x225 - PHASEA0[15:8]: 0x00 0x228 - FREQA1[7:0]: 0x00 0x229 - FREQA1[15:8]: 0x00 0x22A - FREQA1[23:16]: 0x00 0x22B - FREQA1[31;24]: 0xc0 0x22C - PHASEA1[7:0]: 0x00 0x22D - PHASEA1[15:8]: 0x00 0x230 - FREQA2[7:0]: 0x00 0x231 - FREQA2[15:8]: 0x00 0x232 - FREQA2[23:16]: 0x00 0x233 - FREQA2[31;24]: 0xc0 0x234 - PHASEA2[7:0]: 0x00 0x235 - PHASEA2[15:8]: 0x00 0x238 - FREQA3[7:0]: 0x00 0x239 - FREQA3[15:8]: 0x00 0x23A - FREQA3[23:16]: 0x00 0x23B - FREQA3[31;24]: 0xc0 0x23C - PHASEA3[7:0]: 0x00 0x23D - PHASEA3[15:8]: 0x00 0x240 - FREQB0[7:0]: 0x45 0x241 - FREQB0[15:8]: 0x17 0x242 - FREQB0[23:16]: 0x5d 0x243 - FREQB0[31;24]: 0x74 0x244 - PHASEB0[7:0]: 0x00 0x245 - PHASEB0[15:8]: 0x00 0x248 - FREQB1[7:0]: 0x00 0x249 - FREQB1[15:8]: 0x00 0x24A - FREQB1[23:16]: 0x00 0x24B - FREQB1[31;24]: 0xc0 0x24C - PHASEB1[7:0]: 0x00 0x24D - PHASEB1[15:8]: 0x00 0x250 - FREQB2[7:0]: 0x00 0x251 - FREQB2[15:8]: 0x00 0x252 - FREQB2[23:16]: 0x00 0x253 - FREQB2[31;24]: 0xc0 0x254 - PHASEB2[7:0]: 0x00 0x255 - PHASEB2[15:8]: 0x00 0x258 - FREQB3[7:0]: 0x00 0x259 - FREQB3[15:8]: 0x00 0x25A - FREQB3[23:16]: 0x00 0x25B - FREQB3[31;24]: 0xc0 0x25C - PHASEB3[7:0]: 0x00 0x25D - PHASEB3[15:8]: 0x00 0x297 - SPIN_ID: 0x00 0x2B0 - SRC_EN: 0x01 0x2B1 - SRC_CFG: 0x0b 0x2B2 - SRC_TAD[7:0]: 0x00 0x2B3 - SRC_TAD[15:8]: 0x00 0x2B4 - SRC_TAD[23:16]: 0x03 0x2B5 - TAD[7:0]: 0x00 0x2B6 - TAD[15:8]: 0x00 0x2B7 - TAD[23:16]: 0x00 0x2B8 - TAD_RAMP: 0x00 0x2C0 - ALARM: 0x00 0x2C1 - ALM_STATUS: 0x1f 0x2C2 - ALM_MASK: 0x1f
Thank you,
Gil