This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS8327: chain mode

Part Number: ADS8327


Hello,

About the chain mode of ADS8327, it used the separate CS to connect GPIOx of controller, I'd like to confirm if CS could connect together? 

Best regards

kailyn 

  • Hello Kailyn,

    Yes, you can connect all /CS pins together to a single GPIO pin.  You will lose the EOC function.  In this case, after starting a conversion, you will need to delay the maximum conversion time of 1714nsec before pulling /CS low and reading the data out.

    Using the internal clock, the minimum CCLK frequency is 10.5Mhz, or a maximum period of 95nsec.  Each conversion cycle takes 18 CCLK clock cycles, for a maximum conversion time of 18*95nsec=1714nsec.

    Also, since the EOC/INT pin on ADS8327 (#1) is configured as an input (CDI function), you should connect this pin to ground through a 10kohm resistor.

    Regards,
    Keith Nicholas
    Precision ADC Applications