Other Parts Discussed in Thread: ADS1278
Hi team,
My customer tests the EVM board. found some problem.
The customer uses a HIOKI SS7012 to simulate a thermocouple signal. then signal to connect to ADS131M04EVM.
RD setting K type temp setting as 325.4C
RD sees from the GUI that the ADC reading value fluctuates greatly. pic and setting as below. (OSR=1024)
2. Customer set OSR is 16384 then the result as below. (OSR setting 16384)
But the customer is still not satisfied with the results of this test. Due to they compare with ADS1278. Same condition but ADS1278 reading value almost stable .
Customer spec is 0.1C. so they hope to scroll value count< 20.
RD print reading value is shown on the screen. you can see the reading rang is 326.3°C~326.6°C
they hope the reading value very stable even after the decimal point. so can some solution can improve it?