Hi @ all
I'm a bit confused using the file import in the High Speed Data Converter Pro Software.
For test purpose, the ADC is not connected and I would like to use the function "Import binary file".
Could you tell me in which order and format the tool is expecting the samples ?
Currently I'm receiving a bin file including all samples in correct order .. S0 S1 S2 S3 , due to the ADC configuration one sample consists of 12bit and 2's complement.
how do I need to fresh up the samples in order to use the High Speed Data Converter Pro tool properly?
best
Patrick