Other Parts Discussed in Thread: DAC121S101
Hi Team,
my customer plans to replace DAC7512 SOT23 package with DAC121S101. Are there any concerns to do so. The parts are Pin2Pin and have both SPI interface.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Team,
my customer plans to replace DAC7512 SOT23 package with DAC121S101. Are there any concerns to do so. The parts are Pin2Pin and have both SPI interface.
Hi Jan,
I do not see any issue. The specs for the DAC121S101 are mostly the same or better than the DAC7512. Have the customer double check the specs that are critical to their design. The basic operation is the same including the power-on reset to 0V, rail-to-rail voltage output, low power, and power supply range.
Best,
Katlynne Jones