Part Number: DAC38RF82EVM
Hi,
I am trying to use the available Arria 10 reference design for Arria 10 SoC device. The SYNC signal is supposed to come from the DAC EVM and it should be an input for the FPGA. The top design has an input signal named tx_syncn. It is connected to the FPGA pin E24. E24 is connected to an SMA connector named SMA_CLK_OUT (as shown in the schematic of the Arria 10 kit). How the SYNC signal is coming to the FPGA from the DAC? Should it not come from the DAC through the FMC?
What am I missing here? Please help.
Regards,
S. Majumdar