Part Number: ADS8556
Hi team,
The decoupling capacitors connected to AVDD are written in the pin description column as 0.1μF and one 10μF for each pin.
However, Figure 43 on p36 shows a 40μF capacitor connected.
Also, the EVM has six 1μF and one 10μF connected.
What values should I connect as decoupling capacitors?
Please let me know the minimum value and how to connect it.
Also, up to what tolerance should I connect the capacitors?
Sincerely.
Ryu.