Other Parts Discussed in Thread: ADS124S08,
Hi Everyone.
I have designed application PCBA using ADS12480.
I use "Two series Two-Wire RTD, Low side reference measurement circuit " as Attached image.
RTD value I tested 50Ohm. VDD=3.3V, AVDD=4.5V.
I have sent some SPI command to test, but this seem incorrect when I get Output_Code = DA5244(Hex) = 14,307,908(Dec).
Formula: Output_Code = (2^23)*Gain*RTD/Rref = 8388608*16*50/2000 = 3,355,443.
I don't know, why they have a big difference like that?
Beside that, I don't know What value should I config into OSC and SFC register. whether they influence to the result?
Thanks.
Application Schematic
SPI command Test