This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS7038: What difference between ADS7038 and TLA2518?

Guru 11165 points
Part Number: ADS7038
Other Parts Discussed in Thread: TLA2518, , ADS7028

Hi team,

I'd like to consider TLA2518.
However TLA2518 does not have EVM, so I should use ADS7038Q1EVM.

I think ADS7038 mainly added the CRC from TLA2518.
Are there any other different features and SPEC?

Sincerely.
Kengo.

  • Hello,

    TLA2518 is the most basic device in the ADS7028, ADS7038, TLA2518 family. There are several differences between the devices including the temperature ranges and integrated features.

    The ADS7038 is specified over the wider -40C-125C and features the CRC features you noted along with the autonomous monitoring features of the comparator and high/low thresholds.