This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DDC112: Need suggestion for power supply

Part Number: DDC112
Other Parts Discussed in Thread: LM76005
Hello
I want to select a Low Noise Linear regulator to supply 5V power to DDC112 for maximum measurement accuracy.
Input to the Linear regulator will be 12V from DC-DC Buck converter LM76005. Maximum current requirement is less than 300mA.
 
Can you suggest any suitable wide input range low noise Linear/LDO regulator which can provide accurate 5V power to DDC112 ?
Or any other solution to provide power to DDC112 for maximum measurement accuracy ?