Hi,
Can the simulation with TI204c-IP_xilinx.svp do on Vivado?
I tried the TI204c-IP simulation, but I couldn't get the hoping result.
I created a testbench like illustration of "8.1.2 Reference Design Loopback Test Environment" of the TI204c-IP-Users-Guide.pdf(5/17/2021).
*It doesn't use the SYSREF.
*The sys_clk_p & n conects the frequency at 78.125MHz.
*The refclk_p &n conects the frequency at 156.25MHz.
*It displays low of the master_reset_n.
*The qpll0_locked, qpll1_locked and cpll_locked are low.
*I simulated about 20us.
using IP
TI204C-IP-Release-v1.10-LATEST
zc706_8b10b
I tried it on Web pack of Vivado 2019.1.
I changed the device from the xc7z045 to xc7k160, because the Web pack can't compile the xc7z045.