Part Number: ADS7883
My circuit description:
+3.3V VDD
Input is a pulsed square wave of varying voltage, 300us pulse width.
The ADS7883SBDBV is used to measure the voltage of these pulses. I often get accurate measurements. Intermittently, I will get erroneous measurements, but if I make two measurements on the same pulse the second one is always very accurate. Only the first measurement will intermittently be inaccurate. This issue exists only when the input voltage is on the low end.
Question 1: Can you explain what we should expect to see in the measurement data on the first read after coming out of power down. Less accurate measurement? Random Noise? Zero? Other? Is there a reason for the first data not coming out correct?
Question 2: From the datasheet, it looks like the part needs to be powered down using the CS input between the first (invalid data) read and the second read. Is this correct? And if so, is there a minimum/maximum time that the part needs to be powered down for?