Which functions of this chip correspond to which of the three grounds? I assume the ADC inputs sink current to ADC-GND, but I'm not sure if, for example, the DACs use the DGND or the AGND.
Bonus points if you can tell me which specific pin of each ground for each function, if DGND+DGND2 and AGND1+2+3+4 (respectively) aren't tied together internally.
I'm only specifically interested in where the SPI interface sinks its current, and which ground the DAC uses for its reference; however, a full list posted here would be a good resource for engineers that may come across this post later.