Hi, TI Support Team
The following inquiries have been received from customers.
[condition]
AVDD: 3.3V
Ainx: max. 3.3V
The product is being used under the above conditions, but the spec written in the datasheet is confirmed as the maximum value.
1. Is there any possibility of defects when using the product under the above conditions?
2. What is the difference between the FSR part and the Vin part described in the datasheet?
3. When applying the actual product, should the value of Ainx not exceed 3.3V as described in FSR? What problems do you encounter? (eg clipping)
Thanks.
Regards,
MJ