Part Number: DAC38J84EVM
Other Parts Discussed in Thread: DAC38J84
I'm designing my third-party FPGA( XILINX KCU040 kintex ultrascale ) evaluation board with a standard FMC-HPC connector to DAC38J84EVM.
All jumpers at DAC38J84EVM are left untouched.
There are few troubles I encountered and be confued:
1.I connect the EVM through USB to my PC. The GUI shows "CONNECTED".Once I click "1.program and run".The program will run and write data.But once in "Low level view" I click "read register".All data will be set to 1.It seems I canot config it EVEN I try another PC


2.once I connect the 5V Power supply.The LED light will on.Small current sound will be generated from near the LED light.And my power supply voltage will be pull to 3.3V and current ~0.5A.Other LEDs (like D4 -- D7) is never on.

Once I programmed my FPGA,The ALARMS is all on.

is there something wrong?How can I config my EVM board?
Thanks