This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS5294: sampling rate

Part Number: ADS5294

Hi sir,

We would like to run the part at somewhere between 10MHz and 40MHz ADC Clock without using decimation.

Is that possible if we select 10MHz clock rather than 80MHz ADC clock. Is there a min clock adc sampling frequency?

Thanks.

  • Hello,

    As shown in the recommended operating condition table on page 10 of the datasheet, the ADC sampling rate can be minimum 10MHz to maximum 80MHz.

    Hence you can select 10MHz clock in your system.

    Kindly let me know if you have further questions.

    Thanks & regards,
    Abhishek