Other Parts Discussed in Thread: ADC3444, LMH5401
I want to use ADC3444 to digitalize a wide bandwidth analog signal with single polarity from -0.2V~1V. As described in datasheet that "Each input pin (INP, INM) must swing symmetrically between (VCM + 0.5 V) and (VCM – 0.5 V)", so it means that I cannot input this signal single-ended, because signal does not swing symmetrically? Even though the common mode voltage range requirement can be met but the signal still can not input as single end due to nonsymmetric? I am confused with this expression in datasheet. Thanks!