Other Parts Discussed in Thread: ADS1299
Hello guys,
One of my customers is evaluating ADS1299-4 on their own board for their new products.
They measured several resistor values using the input circuit like the attached PDF.
The result is the follow.
External resistor Difference voltage between Converted resistor value
value (kohm) the resistor terminals (V) from read out data (kohm)
10 0.0576 10.07
56 0.319 53.33
100 0.568 94.49
200 1.110 185.36
300 1.625 273.15
400 2.117 353.18
560 2.313 384.87
1000 2.386 396.35
At this moment, they have the following questions.
Could you please give me your reply for them?
Q1. As the external resistor value increases, the errors between actual value and converted resistor value are increased in the negative direction.
Do you think what the cause is? Is it the internal current source (6uA) error? Does the source current decrease when INP voltage is increased?
Q2. Should the internal current source be used for Lead-Off detection only?
Q3. Do you have any recommended circuit for external resistor value measurement?
Your reply would be much appreciated.
Kazuya.