Part Number: AFE0064
Other Parts Discussed in Thread: AFE2256, ADS8363, AFE2256EVM
Hi Experts,
Good day. We have a raised queries a follows:
1. Can we use 2 AFE0064 ICs to read from a 128 channel input device? If, yes, how do we do it and what extra circuit do we need?
2. If we want to read the output of AFE0064 using a AFE2256, do we need extra ADCs in between ? If yes, which one are suitable for high speed operation and if not, why?
3. The input to our AFE0064 is going to be currents (in nano amperes), both positive and negative. Will that be okay?
4. We wish the scan time of our circuit to be as least as possible. The maximum data transfer rate of AFE0064 is 7.5 MHz. If possible, we would like to achieve this maximum data transfer rate from our device to PC. Can we do that?
5. Do we have any evaluation board for this IC? (probably not have)
Thanks for your guidance.
Regards,
Archie A.