Other Parts Discussed in Thread: THS4541,
HI Sir
which one is correct? thanks

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
The image on the left is the most correct since the differential input pins (AINP and AINM) can swing from +1.125V to - 1.125V. The differential signal swing is (+1.125V - (-)1.125V = 2.25V). These voltages must both include the +0.95VDC common mode voltage (VCM) which can be supplied from the ADC pin VCM.
The THS4541 fully differential amplifier is used on the ADC3643EVM to provide the differential input (with the VCM) to ADC analog inputs. Please see the ADC3643EVM for an example of how to use the THS4541.
Best Regards,
Dan