Hi,
Can I interface SiPM (avalanche photodiode) directly to the input of DDC232 to convert the current to voltage?
Regards,
Mike
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
Can I interface SiPM (avalanche photodiode) directly to the input of DDC232 to convert the current to voltage?
Regards,
Mike
Hello Mike,
I wanted to let you know that our expert on this device is out of the office for Christmas and New Year holidays, he will be back in the office on 1/3/22.
Thank you for your patience.
Hi Mike,
Thanks for the patience.
With my limited knowledge on the SiPM sensor, I do not see why not. However, can you please help to describe what kind of signal you expect from the SiPM avalanche photodiode connected to the DDC23?. Your attached diagram shows it will be a current pulse that needs to be converted to a voltage pulse with the ADC.
The DDC232 operates based on integrating the input current for a specific amount of time and convert the charge collected to digital output with the ADC. Please refer to the DDC232 datasheet for the device's basic operation and see if it is suitable for your application.
Thanks
-TC
Hi TC,
Please see the SiPM operation at the following link:
What is an SiPM and how does it work? | Hamamatsu Photonics
Also, what is the maximum current that we can have at the analog input of DDC232?
Regards,
Mike
Hi Mike,
Thanks for the information on the SiPM sensor.
The DDC232 has 7 input ranges from 12.5pC to 350pC. Please refer to the E2E post below for a more detailed explanation on the relationship between the analog input current and the integration time for the DDC devices.
Thanks
-TC