Other Parts Discussed in Thread: LMK04828, ADS54J64
Hi,
I have both the ADS54J64EVM and TSW14J56EVM boards connected to each other and I have the example design running as described in section 2.2. I used my ZC706 Zynq-7 eval board to provide the 61.44MHz clock reference to the LK04828. Now I would like to put the LMK04828 into clock distribution mode per section 3.2 of ADS54K64EVM manual so that I can have the ADC sampling rate equal to the frequency at LMK_CLK_IN. The manual states that there is a Macro State Script LMK04828_config1.cfg to do this but it does not explain at all how to load it. The manual does state "If it is required to operate the LMK04828 device in clock distribution mode, the onboard VCXO must be disabled by removing the shorting jumper at JP2." which I can easily do but I am not sure how to program the LK04828 and the CPLD on the ADS54J64EVM to put the board into clock distribution mode and have the ADC sampling frequency at my LMK_CLK_IN frequency.
Thank you,
Keira