Hello,
For the ADC128S102QML, can you confirm that an external sampling clock is not required? How is the sampling frequency set between 50 kSPS and 1 MSPS?
Thank you
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
For the ADC128S102QML, can you confirm that an external sampling clock is not required? How is the sampling frequency set between 50 kSPS and 1 MSPS?
Thank you
The ADC128S102QML-SP product does not require a free-running clock for operation. The ADC acquisition and conversion timing which determine the sampling rate are all based on the SPI interface timing. High frequency (16MHz) SCLK signals result in the full 1MSPS sampling rates and a slower (50kSPS*16clks/sample) = 800kHz SCLK would result in the 50kHz sampling rates. The first 3xSCLKs define the Track/Acquisition period and the remaining clocks are used for the conversion/hold phases.
Hello,
We offer this information on the device product folder in the Design & development section. I copied it below for easy reference.
For additional terms or required resources, click any title below to view the detail page where available.
Package | Pins | Download |
---|---|---|
(Y) | 0 | View options |
CFP (NAC) | 16 | View options |
CFP (NAD) | 16 | View options |
Hello, The CAD data for the NAC package does not work, can you check what has been uploaded to Ultra Librarian please.
Kind Regards,
Rajan
Hello Rajan,
I have submitted a ticket with the owners of that tool to look into the situation. Would you confirm the error/challenge you experienced along with the CAD tool you were using to view the information?