Hi,
I'm having issues connecting the the TLA2024EVM via the GUI. It appears as though the device connects for 1 or 2 seconds (green indicator with 'device connected' status) then a 'Connection Failure' message appears. I believe I am using the correct GUI, TLA2024EVM_GUI, and I have also manually installed the 'Generic Bulk Device' driver which did not install correctly originally though the TICloudAgent installation, but although there is no longer a warning next the the 'Generic Bulk Device', I am not convinced it is properly installed. Is there any further trouble shooting for this EVM that can be done?