Other Parts Discussed in Thread: AFE5832, LMK04821,
Hello,
I am using the TSW1400EVM with the AFE5832 EVM. I try to set up the first test setup like in the AFE5832 Userguide section 4.2: Capturing Analog Input signals with LVDS interface (https://www.ti.com/lit/ug/slou489/slou489.pdf?ts=1641804892305&ref_url=https%253A%252F%252Fwww.ti.com%252Ftool%252FAFE5832EVM). After downloading the firmware and configure the device, USER LED5 and USER LED6 are off and all others are on. I try to capture data in HSDC Pro but the following error messages appear: Read DDR to file TIMED_OUT_ERROR. Instead of an external clock I am using the differential outputs from LMK04821. As USER_LED3/D5 is on, so it is no clocking issue?
I use the following software: HSDC Pro v4.7 and AFE5832 GUI v1.0.0
Hardwaresetup: like in the AFE5832 Userguide with: 5 V (4A) power supply, Signal generator 5 MHz -20dBm on SMA J1, clock jumpers as in configuration 3 with Y2 (figure 63), Jumpers on J41/J53/J57
The settings in the GUI are the following:
Thank you very much for your help