This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AFE5808A: AFE5808A DNC pins at L6、M6、L7、M7

Part Number: AFE5808A


Dear TI experts:

    As regards to  the AFE5808A, i have some questions about the DNC pins, which are listed below. Could you kindly give me some help on this?

Thanks in advance!

Detailes of question:

Q1:  what's insde the chip of the DNC pins at L6、M6? Could i connect 1.8V to the DNC pins at L6 and M6?

Q2: what's inside the chip of the DNC pins at L7、M7? Could i connect GND or 2.5V to the DNC pins at L7 and M7?

Eagerly expecting your reply.

Best regards,

eric