Part Number: TSW1400EVM
Hi,
I wanted to automate the continuous capture function to store subsequent samples of data in different files or continuously writing it in a same file (which I can later make it into separate files knowing the number of samples per capture). So my basic requirement is to turn on the continuous capture function during a particular time that I desire and keep writing them to files until a stop command is issued (just similar to using the capture button and saving the captured data to a file when continuous capture is running in the GUI) and the problem arises as I am not able to find an automation script for continuous capture.
Regards,
Adithya N
Email: adithya.n@galaxeye.space