Part Number: ADS1282-SP
Other Parts Discussed in Thread: ADS1282
Dear all,
I have some question about Power-ON Sequence.
ADS1282-SP has 3 power supplies: AVDD, AVSS and DVDD.
Datasheet says that there is no specific order applicable to device power supplies; then it says that internal reset is removed when AVDD-AVSS and DVDD exceed 3.5V and 1V, respectively.
Somewhere else is written that SPI could start improperly and require a dedicated reset procedure to make the device correctly reading SCLK.
I would like to have confirmed that I can cycle AVDD-AVSS without removing DVDD without damaging or improperly starting the device.
Thank you in advance.
Daniele