Hello,
I have to find a way to measure the leakage current of GaN or SiC-Mosfets in a HTRB test. These currents are in the range of 15nA to 1mA and therefore the voltages at the input of the ADC will be minimal and would require a high amplification and noise rejection. Due to the device under tests that we use, the voltage over the switches can get as high as 6kV. Do you have any clue about a possible Transimpedance-Amplifier + ADC and Schematic that I could use for this use case?. Additionally I will have to think about the isolated power supply and SPI lines.
Thanks,
Javier