Could you please help me to calculate the correct ENOB for ADCS7476? I am expecting a result below 12, but not sure which parameter to include in the notorious formula:
ENOB=(SINAD-1.76)/6.02
Shall I consider the minimum value of SINAD=70, given in table 6.5 in the datasheet? Or to use the minimum value of SNR (70.8 below 85°C or 70.6 for 125°C). Or maybe I need to consider the SINAD value in figure 12 from the datasheet (for 1MSPS)?
I would like to understand how ENOB value is correctly calculated during a normal ADC selection process. For this particular ADC I have a "calculated value" of ENOB = 11.66, but can't figure it out how is calculated.
Any help is appreciated! Many thanks in advance!