Hello,
We developed EEG device by using ADS1299.
When applying +/-150mV DC offset voltage to the channel in series ,however, we obseved undesired 50Hz signal.
Although our area's line frequency is 50Hz ,observed 50Hz signal differs from line frequency.(Graph 1)
This signal level depends on the DC offset voltage level. (Table 1 and Graph 2)
I attach the test circuit(test circuit.pdf) ,measured data(data.pdf), and register setting(register.txt).
We want to know if applying series DC offset voltage to ADS1299 causes this problem.
Best regards,
test circuit.pdf data.pdf
address value
00h 3Eh
01h 96h
02h C0h
03h ECh
04h 0Ch
05h 68h
06h 68h
07h 68h
08h 68h
09h 68h
0Ah 68h
0Bh 68h
0Ch 68h
0Dh FFh
0Eh FFh
0Fh 00h
10h 00h
11h 00h
12h 00h
13h 00h
14h 0Fh
15h 00h
16h 00h
17h 00h