Other Parts Discussed in Thread: ADS124S06
I can't find answer to my question in the datasheet. For example, I measure 0.1 VDC with gain 1 and gain 16. What's the maximum error between two values I can expect? What about all gains from 1 to 128 (of course, the VDC at input will be lower)
ADC power supply is +3.3V at AVDD and -1.24 at AVSS. Data rate is 20 SPS. I do selfcal before measurement. I also user an internal reference voltage source.
As I understand the 'gain error' at the datasheet says about gain linearity not the difference in measurements between several gains?
For example, I gave 0.1 VDC linear source powered from 18650 Li-po (so, no noise, no ripples) and I have next results:
PGA Measured Value, mV
1 0.99957
2 0.99961
4 0.99928
8 0.99994
16 0.99899
As we see at the best gain (more gain,more scale is used) we have 'strange' result. So, why the error between first for (1, 2, 4, 8) gains is small, and it is so big between the fifth (16) gain and first four gains?
I'm not interested in measurement of absolute value, only in ratio between gains...