This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Experts,
Our customer thinks of using DAC5670-SP but he is looking for Evaluation Board available for this part?
And as I check the product folder, there is no available EVM for this.
Is there no other EVM that is compatible and can be use for DAC5670-SP?
Customer also ask, if we don't make an Evaluation Board for the DAC5670-SP what is the closest device with an EVM?
I check DAC12DL3200 as it have EVM. Is this the closest product that we can suggest?
I hope to get advise from you. Thank you so much.
Kind regards,
Gerald
Hi Gerald,
Can the customer please come back with the criteria on the DAC and we can help down-select an appropriate device.
If the customer is looking at the DAC5670-SP. Do they need a space qualified device? That will help narrow the search if so.
Regards,
Rob
Hi Rob,
I was able to confirm that yes, customer need a space qualified device. He plan on using the DAC5670-SP. Does the DAC5670-SP have an evaluation board? As I check the product folder, there is no available EVM. Since it does not then which part would have an EVM that comes closest to the DAC5670-SP? He want to use the schematic of such an EVM to help with the design of the DAC5670-SP. Thanks
Kind regards,
Gerald
Hi Rob,
I find DAC5675A-SP as a close device having same resolution, reference type, interface type and is also a space grade but only have sample/update rate of 400MSPS. I also check that it have an EVM. Is this the closest product that we can suggest? Please let me know if you have better suggestion for the closest device to DAC5670-SP that have EVM. Thank you so much.
Kind regards,
Gerald
Hi Gerald,
Let me see what I can verify for you the customer. Please give me a few days.
Regards,
Rob
Hi Rob,
Thank you for your attention on this. We will be waiting for your reply.
Kind regards,
Gerald