A quick look at the datasheets suggests the 12 bit device would drop in to a design for the 10 bit device.
Can you confirm this is the case?
Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
A quick look at the datasheets suggests the 12 bit device would drop in to a design for the 10 bit device.
Can you confirm this is the case?
Thanks
Hi Adrian,
Yes, they are pin compatible and the 12-bit can drop in for the 10-bit. The write sequences will remain the same. If your code is writing the last two data bits as zero, then the 12-bit device will behave as a 10-bit device.
Best,
Katlynne Jones