Part Number: TSC2004
Hi, thanks in advanced for any kind of help
Im considering to add the TSC2004 to my design and due is a battery device, consumption is always my bottleneck.
I do not have experience with such controllers and i need it to detect all the time possible actions on the resistive panel.
I saw on datasheet that at 1,17KsPs with Vref=1,2V i can achive the lowest consumption of 39,4uA . For me this is a huge problem for my standby mode.
Then i saw this power down mode (0,023uA). My question is, if the device is in power down mode, i have no option than to use PINTDAV as interrupt to awake the host right?, besides to switch ON every X miliseconds or seconds. Is that correct?
Are no other option to decrease this stanby consumption but sampling the touch? because i can not say to the client, first you need to touch it and then enter the codes.
Maybe other controller from TI can help me with the consumption?
thanks!