Part Number: ADS4142EVM
Hi,
I'm using ADS4142EVM board.
I am applying a 200mV amplitude sine wave from a 50-ohm signal generator to J6 input of the EVM (Single Ended). I am not applying any DC.
The output at the software of the evaluation board (TSW1405EVM) is -16 dBFS.
I thought : 20*log(200m/1)= -14 dBFS but I am getting -16 dBFS.
My questions :
1. Why am I seeing 2 dB difference? Is it correct to use 1 in the denominator?
2. Is the input is 50-ohm matched?
PS: I am using the default setting on the "High speed data converter pro" software with 65536 samples (Analysis window) at 10-MHz sampling rate.