Part Number: ADC3683
Other Parts Discussed in Thread: TDA4VM
Hi TI,
the ADC3683 datasheet mentions in chapter 8.5 Programming, that "The device is primarily configured and controlled using the serial programming interface (SPI)". When looking up the specification of this interface, I found some differences to the more common known Serial Peripheral Interface (SPI):
Serial Programming Interface Signals: SCLK, SDIO
Serial Peripheral Interface Signals: SCLK, MISO, MOSI
So if I want to configure/control ADC3683 via Serial Programming Interface, is it recommended to connect it to Serial Peripheral Interface (e.g from TDA4VM SoC)? If not, which changes do I need to make to drive Serial Programming Interface via Serial Peripheral Interface? Is I2C also an option?
Thanks for your help and best regards,
Felix