1. can ADS52J90 input a pure DC signal (yes /no)?
2. can ADS52J90EVM input a pure DC signal (yes /no)?
3. which TI multichannel device can input DC signal?
much appreciated,
Ehud.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
1. can ADS52J90 input a pure DC signal (yes /no)?
2. can ADS52J90EVM input a pure DC signal (yes /no)?
3. which TI multichannel device can input DC signal?
much appreciated,
Ehud.
Hi Ehud,
1. can ADS52J90 input a pure DC signal (yes /no)?
Yes, the input frequency range is 0 - 70 MHz.
2. can ADS52J90EVM input a pure DC signal (yes /no)?
Yes.
3. which TI multichannel device can input DC signal?
I believe almost all SAR adcs can measure DC signals. You can refer to the following webpage to browse through multichannel ADS products.
https://www.ti.com/data-converters/adc-circuit/overview.html
Thanks & regards,
Abhishek