Hey guys, does TI have similar product to PI3PCIE3442A.
The data sheet is here. It is 8-differential channel 2-lane exchange. It is PCIe cross-switch which I am planning to use for USB3.0. I am curious if TI has similar product.
Thanks in advance!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hey guys, does TI have similar product to PI3PCIE3442A.
The data sheet is here. It is 8-differential channel 2-lane exchange. It is PCIe cross-switch which I am planning to use for USB3.0. I am curious if TI has similar product.
Thanks in advance!
Our group don't have such cross-switch.
Regards
Brian
Hello,
One option would be to look into the TS2PCIE2212. The operating VCC is different, but has similar crosspoint operation otherwise. In addition, you can try to look into the HD3SS3412...not exactly a crosspoint switch, but has similar specifications.
Thanks!
Bryan
It seems TS2PCIE2212 does not have the same functionality PI3PCIE3442A. The PI3PCIE3442A has truth table as below: Ax = Bx, Cx = Dx when E=0 and Ax = Dx, Cx = Bx when E=1. Truth table for TS2PCIE2212 is Ax = Bx, Cx = Dx when E=0 and Ax = Dx, Cx = N/A when E=1.
Please correct me if I am wrong.
Thanks for the responses!
Hello,
You are correct, the device only has similar functionality as it is not exactly the same. We do not offer a device that is exactly like the device mentioned.
Thanks,
Bryan