Hello,
If I have a project working with ADS1113IDGS, I can just solder a ADS1113BQDGSRQ1 without modifications in the firmware of the project?
They are 100% firmware compatible?
Greetings
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
If I have a project working with ADS1113IDGS, I can just solder a ADS1113BQDGSRQ1 without modifications in the firmware of the project?
They are 100% firmware compatible?
Greetings
Hi user6364479,
yes, those two devices are 100% firmware, pin and functional compatible.
Regards,
Joachim Wuerker