Part Number: TLA2518
Hi team,
In the TLA2518 datasheet there is no mention that I can find of the calibration time. For calibration, all I see is what is given in 7.3.4:
The variation in ADC offset error resulting from changes in temperature or AVDD can be calibrated by setting the CAL bit in the GENERAL_CFG register. The CAL bit is reset to 0 after calibration. The host can poll the CAL bit to check the ADC offset calibration completion status.
Is there a maximum calibration time or a way to calculate the maximum calibration time?
Thanks,
Jacob