This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

WAVEVISION5: A/D card

Part Number: WAVEVISION5
Other Parts Discussed in Thread: ADC3541, ADC3563, ADC3583

Hi Team,

Our customer is looking for an A/D card to read out the DC voltage level (voltage signal from photodiode fed with coaxial cable, photodiode signal will be AC 1.5 MHz + DC voltage level). Kindly refer to the set-up below. 

I checked our product offerings and I found the WAVEVISION system. However, as I read the User's manual, I found that this system is used for TI's ADC and DAC evaluation boards. Can the customer also use this to their application above? if not, Could you please suggest a solution?.

Thank you in advance.

Regards,

Marvin